Browse FAQs

What is the part number for the Micro 110CPU modbus programming cable?

Published date: 31 July 2019

Issue
Part number for programming cable

Product Line
Modicon Micro

Resolution
The part number for the Micro 110CPU modbus programming cable is a 110XCA20300 (DB9 - RJ45 Adapter) and one of the below 110XCA2820X  communication cable depending of length needed:


110XCA28201 RS232 Communication Cable—3ft, RJ45–RJ45.
110XCA28202 RS232 Communication Cable—10ft, RJ45–RJ45.
110XCA28203 RS232 Communication Cable—20ft, RJ45–RJ45.

Was this helpful?

What can we do to improve the information ?

Can't find what you are looking for?

Reach out to our customer care team to receive information on technical support, assistance for complaints and more.