Browse FAQs

Does Schneider Electric offers a Magelis HMI rated for wash downs?

Published date: 22 October 2018

Issue:
Does Schneider Electric offers a Magelis HMI rated for wash downs?

Product Line:
washdown, Magelis, HMIGTO, stainless steel

Resolution:
Yes, HMIGTO2315/5315/6315 which has the stainless steel bezel are rated for wash down of water jet pressure up to 128 psi ( 1 bar = 14,5 psi ).
 

Was this helpful?

What can we do to improve the information ?

Can't find what you are looking for?

Reach out to our customer care team to receive information on technical support, assistance for complaints and more.