Technical FAQs

Ask a Question

Which SD card slot do I use to do a File System transfer on a Magelis HMIG3U?

The HMIG3U has 2 SD card slot. The System SD card use for the Runtime and the Secondary storage SD card.
The File System transfer on a Magelis HMIG3U is done though the secondary drive (SD card) or optional drive (USB Flash drive) on the HMIG3U.
 
Was this helpful?
What can we do to improve the information ?