Technical FAQs

Ask a Question

Is there a list of error codes for the Preventa XPSMCM Safety Controllers?

Issue:
Is there a list of error codes for the Preventa XPSMCM Safety Controllers?

Product Line:
XPSMCM, SoSafe, Preventa, Safety

Environment:


Cause:


Resolution:
Below are a list of error codes:
CODE FAIL SOLUTION
  1D :  31D Microcontroller Error Try to Restart System. If Error Persists, send unit to our Expert Assessment Center for making a  =S= expertise report following the  Return for Technical Expert Assessment (RTE) process.
32D :  63D Main board Error
64D :  95D Communication Error between units
96D : 127D MCM memory card error Replace MCM memory card
128D : 138D Error module R04/R04DA relay 1 Try to Restart System. If Error Persists, send unit to our Expert Assessment Center for making a  =S= expertise report following the  Return for Technical Expert Assessment (RTE) process.
139D : 148D Error module R04/R04DA relay 2
149D : 158D Error module R04/R04DA relay 3
159D : 168D Error module R04/R04DA relay 4
169D : 191D Error units EN encoder interface
192D : 205D OSSD1 Error
206D : 219D OSSD2 Error
220D : 233D OSSD3 Error
234D : 247D OSSD4 Error
Was this helpful?
What can we do to improve the information ?