Browse FAQs

Can I set the up / down arrow buttons on an ATV61 for + /- speed?

Published date: 25 July 2019

Issue: 
ATV61 can I set the up / down arrow buttons for  + /- speed?

Product Line:
ALTIVAR 61

Environment:
 All 

Cause:
Installation / Setup

Resolution:
No, the ATV61 intergrated up/down arrow buttons cannot be configured for (+) / (-) speeds. 

Was this helpful?

What can we do to improve the information ?

Can't find what you are looking for?

Reach out to our customer care team to receive information on technical support, assistance for complaints and more.