Browse FAQs

Which of the four VIEWS does ProWORX 32 use when printing?

Published date: 29 July 2019

Issue
Printing views

Product Line
ProWORX 32

Resolution
ProWORX 32 was designed so it only chooses the first view configured "VIEW 1" when printing. VIEWs 2, 3 and 4 can be used for viewing in the logic program but cannot be used for printing purposes.

Was this helpful?

What can we do to improve the information ?

Can't find what you are looking for?

Reach out to our customer care team to receive information on technical support, assistance for complaints and more.