Technical FAQs

Ask a Question

Osisense XC - Equivalent of the XCKJ267 limit switch

The XCKJ267 limit switch reference has been discontinued in the 1990's, no more available in 2016. It has to be ordered by the sub-assemblies ZCKJ2 body + ZCKE67 head. The XCKJ267H7 limit switch is available to order in 2016, it is a product manufactured to order. To get the XCKJ267H29 limit switch, order both sub-assemblies ZCKJ2H29 + ZCKE67.

Was this helpful?
What can we do to improve the information ?