Technical FAQs

Ask a Question

What is the ordering number for the Profibus connectors used with Lexium Integrated Drives that have industrial cover ?

The Profibus connectors come as a set of three pieces.
The ordering reference number for the set is VW3L5B000

Included in the set will be:
1 - Male M12 B-coded profibus connector
1 - Female M12 B-coded profibus connector 
1 - Blanking plug ( used to cap the profibus out connection on the last device in the network )

Rev 11-28-17
Was this helpful?
What can we do to improve the information ?