Technical FAQs

Ask a Question

What is one of the more common reasons for not being able to communicate via USB with an open Unity project ?

One of the more common reasons is that the project is in Simulation Mode. The project must be in Standard Mode in order to communicate via USB.
Was this helpful?
What can we do to improve the information ?