Technical FAQs

Ask a Question

PlantStruxure PES [V4.1]: How to make $MBClientBasic template to read/write IW registers?

For PES v4.1 or later:  go into "propertise" of template "MBClient", and chose the "Typer of register" as "TURE". (see the following picture)


For PES v4.0 SP1: There is no the option "Type of register" in propertise of $MBClient, we need to set the pin "Memory Input" of MBClient to "1" in Unity Refine: (see the following)


 
Was this helpful?
What can we do to improve the information ?