Browse FAQs

Does Schneider Electric offer accessory cables for use with Berger Lahr N065 motors?

Published date: 03 October 2018

No,  The Icla N065 and ICLA D065 are very old legacy products which are no longer offered in our catalogs.
Therefore there are no accessory cables offered for use with the Berger Lahr N065 integrated drive type motors.

Icla N065 and Icla D065 motors are still available for support of old machines.

However, all cables used with Icla N065 and Icla D065 are required to be fabricated if needed.

Rev 9-20-17

 

Was this helpful?

What can we do to improve the information ?

Can't find what you are looking for?

Reach out to our customer care team to receive information on technical support, assistance for complaints and more.