Technical FAQs

Ask a Question

What is the maximum length that the cellular modem antenna can be located from ION8650?

Issue
The antenna may need to be located in another location than the ION8650 meter.

Product
ION8650

Environment
Installation

Resolution
The ION8650 is connected to the antenna via an SMA connection. This connection can be extended to 12 feet using an SMA to SMA cable.
Was this helpful?
What can we do to improve the information ?