Technical FAQs

Ask a Question

How to access websites that requires authentication using XML Import Module?

Product Line
ION Enterprise 6.0.x
StruxureWare Power Monitoring 7.0.x
Power Monitoring Expert 7.2.x, 8.x

Environment
Designer, VIP

Resolution

The XML Import Module does not provide a location to specify a user name and password, however the following URL format can be used, provided the website in quesiton supports basic access authentication. 

http://username:password@www.example.com



 
Was this helpful?
What can we do to improve the information ?