Browse FAQs

What is the Maximum distance between X80 I/O racks using the Extender Module BMXXBE1000 on an M340 or M580 system?

Published date: 29 July 2019

Issue:
My extension racks are not operating properly. What is the maximum length of the extender cabling?

Product Line:
M340, M580, X80 IO

Environment:
Ecostruxure Control Expert
Unity Pro

Resolution:
The cumulative length of all the extension rack cables in the PLC application is limited to a total of 30m.

Was this helpful?

What can we do to improve the information ?

Can't find what you are looking for?

Reach out to our customer care team to receive information on technical support, assistance for complaints and more.