Technical FAQs

Ask a Question

Does Schneider Electric offer a direct replacement for Berger Lahr motor type IFE71/2CAN-DS/-QBB54/2-064KSP54 with ID number of 66307190016

No, the Berger Lahr motor type IFE71/2CAN-DS/-QBB54/2-064KSP54 with ID number of 66307190016 is a special version for Atlas Converting in Europe
There ares some design features incorpoprated in this model which are unique to the OEM Atlas
This model uses a 64:1 gearbox which is not included in our standard offer.
The customer must contact the OEM machine builder in Europe for spares.

rev 11-6-20
Was this helpful?
What can we do to improve the information ?