Technical FAQs

Ask a Question

When will the Magelis Panel PCs 10”, 15”, 19” Magelis Box PCs be obsoleted and what replaces them?

Industry business announces the obsolescence of the following Magelis iPC ranges in December 2016. - Magelis Panel PCs - 10", 15 and 19" (Catalog numbers starting with HMIPW, HMIPU, HMIPP with aluminum bezel and HMIPR, HMIPT, HMIPF with stainless steel bezel) - Magelis Box PCs (Catalog numbers starting with HMIBU and HMIBP) - All Configured iPCs with Windows XP (HMIPCC*1*) . Please refer to the attached document for replacement part numbers.

For specific model replacement part numbers and cutout information for the the replacement IPC see the attached spread sheet PanelAndBoxPC_Transition Tool.xlsx
Was this helpful?
What can we do to improve the information ?