Technical FAQs

Ask a Question

Query for determining when an ION Meter has had a power cycle

Issue
The attached query will provide a listing of all instances in which an ION meter lost it's control power and the duration of that outage. 

Product Line
StruxureWare Power Monitoring 7.0.x
Power Monitoring Expert 7.2.x, 8.x

Environment
SQL Server Management Studio

Resolution

*Warning: Irreparable database damage can occur. This procedure should only be performed by users familiar with SQL Server Management Studio. Databases should be backed up prior to performing this procedure.*


1) Open the following query in SQL Server Management Studio
2) Execute the query

The results of the query provide the following information: 
Meter Name
Date / Time of the Power Down Event (in UTC)
Duration of the outage


 
Was this helpful?
What can we do to improve the information ?