Technical FAQs

Ask a Question

Does the XBTZGUMP, USB Modbus Plus converted, supported by the HMIG3U?

Issue:
Does the XBTZGUMP, USB Modbus Plus converted, is supported by the Magelis HMIG3U target?

Product Line:
HMIGTU, HMIG3U

Environment:


Cause:


Resolution:
Yes, the XBTZGUMP is support by the HMIG3U target.
Was this helpful?
What can we do to improve the information ?