Technical FAQs

Ask a Question

Are the Magelis HMIGTO rated for Class1 Div2?

Issue:
Are the Magelis HMIGTO rated for Class1 Div2?

Product Line:
Magelis, Class1 Division2

Environment:


Cause:


Resolution:
Yes, the Magelis HMIGTOs are rated for Class1 Div2.
Was this helpful?
What can we do to improve the information ?