Browse FAQs

Why doesn't the Quantum CPU show up in the Proworx 32 traffic cop?

Published date: 31 January 2019

Issue
Quantum CPU does not show up in Proworx 32 traffic cop

Product Line
Proworx 32

Resolution
The Quantum CPU doesn't show up in the Proworx 32 traffic cop when you create a new Proworx 32 Project and then go online and do a "Read" from Controller. You can always add the Quantum CPU in the traffic cop.

Was this helpful?

What can we do to improve the information ?

Can't find what you are looking for?

Reach out to our customer care team to receive information on technical support, assistance for complaints and more.