Browse FAQs

When will reading and writing to Rockwell RSLogix UDT tags be supported in Vijeo Designer?

Published date: 14 June 2019

Issue:
When will reading and writing to Rockwell RSLogix UDT tags be supported in Vijeo Designer?

Product Line:
Vijeo Designer V6.2

Resolution:
Reading and writing to Rockwell RSLogix UDT tags over Ethernet / IP is supported starting from Vijeo Designer V6.2 SP5 or higher.

Was this helpful?

What can we do to improve the information ?

Can't find what you are looking for?

Reach out to our customer care team to receive information on technical support, assistance for complaints and more.