Technical FAQs

Ask a Question

Power requirements for the Connexium Fiber SFP modules used with the Connexium TCSESM103F2LG0 switch

The following Connexium Fiber SFP modules do not require an external power source they get powered through the switches power source.
TCSEAAF1LFU00   Fiber Module SFP-SX/LC.
TCSEAAF1LFS00   Fiber Module SFP-LX/LC.
TCSEAAF1LFH00   Fiber Module SFP-LH/LC.
Was this helpful?
What can we do to improve the information ?