Technical FAQs

Ask a Question

Preventa XY2C - XY2CZ201 cable with red sheath cross-reference

The obsolete XY2CZ201 cable with red sheath is replaced by the XY2CZ301 one (same lenght 10.5m). The difference is the cable diameter : XY2CZ201 dia 2.2mm; XY2CZ301 dia 3.2mm.

Was this helpful?
What can we do to improve the information ?