Technical FAQs

Ask a Question

Osisense XC - What is the ZCKJ533 part number? How to replace?

The ZCKJ533 contact body is the ZCKJ5 contact body having the front cover ZCKZ033, which is the XCKJ limit switch cover + indicator light module, with 2 neon lights 110V-120V AC. Attached corresponding picture. Please note this contact body ref. is discontinued since 2014 and replaced by the equivalent ZCKJ534 contact body = ZCKJ5 having the ZCKZ034 cover + indicator light module 2 LEDs 110-240V AC.

Was this helpful?
What can we do to improve the information ?