Technical FAQs

Ask a Question

Does Schneider sell the KAB-3225-LI Interbus cable in the US?

Schneider Electric USA does not stock or sell trunk cable for Interbus-S. 
In Europe this part may be ordered thru Schneider Electric Germany. Part Number KAB3225LI

In North America these cables can be ordered thru Belden.
Part Number 3119A is a 6 conductor plus another pair for power.
Part Number 3120A is a 6 conductor cable.

These cables come in 500 foot or 1000 foot lengths.

Was this helpful?
What can we do to improve the information ?