Technical FAQs

Ask a Question

Can the HMISCU controllers be used without the display?

Issue:
Can the HMISCU controllers be used without the display?

Product Line:
HMISBC, HMISAC, HMISCU8B5, HMISCU6B5, HMISCU8A5, HMISCU6A5

Environment:


Cause:


Resolution:
That is not possible, the HMISCU controller requires a front display to function properly.
 
Was this helpful?
What can we do to improve the information ?