Technical FAQs

Ask a Question

Osisense XC - Special dia 50mm roller lever ZCKY422460 data sheet

Please find attached the special variable lenght thermoplastic roller dia 50mm lever ZCKY422460 definition and dimensions. It is not shown into the Osisense XC standard catalogue. Such special lever is dedicated for the XCKS limit switches model. It is in fact a ZCKY49 lever with a rigid POM roller. Logistic situation in 2016 : available to order. It is a MTO product (manufacture to order).

                   
Was this helpful?
What can we do to improve the information ?