Browse FAQs

Can a Quantum IO module be hot swapped?

Published date: 26 October 2018

Yes. However this must be done by a qualified individual who is familiar with the inputs or loads associated with the module.
You need to be aware of how the loss of signal input or control output can effect the application before performing the swap.

The Quantum CPU's,standalone CPS,CHS and CRP modules should never be hot swapped.

 

Was this helpful?

What can we do to improve the information ?

Can't find what you are looking for?

Reach out to our customer care team to receive information on technical support, assistance for complaints and more.