Technical FAQs

Ask a Question

Can a port number other than Modbus/TCP port 502 be used for Modbus messaging in the 140CPU6xxxx native ethernet port?

No.. The Quantum 140CPU6xxxx CoPro Native Ethernet port will only use Modbus TCP port 502 for Modbus messaging.
Was this helpful?
What can we do to improve the information ?