Technical FAQs

Ask a Question

Preventa XY2C - Adapted rope pull switch XY2CJS15S03 datasheet

The adapted rope pull switch XY2CJS15S03 is based on the standard E.stop rope pull switch XY2CJS15 having cable entry M20, with the following specificity : add a 5-pin M12 connector in the M20 threaded entry. Logistic situation in 2016 : available to order without any marketing restriction, MTO product (MTO = manufacture to order).

Was this helpful?
What can we do to improve the information ?