Technical FAQs

Ask a Question

What would be the solution to connect a Magelis application using IEEE 1394 interface

Today we have no such connection for the IEEE 1394 interface on the Magelis series of HMIs

XBT, HMIGTO, HMIGTU, HMISTO, HMISTU series.
Was this helpful?
What can we do to improve the information ?