Technical FAQs

Ask a Question

Can the USB tower light, part number XVGU3SHAV, be used without the Magelis?

Issue:


Product Line:


Environment:


Cause:


Resolution:
No, this particular USB tower light is made specifically for the Magelis and needs to be programmed with Vijeo Designer.
Was this helpful?
What can we do to improve the information ?