Technical FAQs

Ask a Question

Is there a conformal coating option for the Magelis HMIGTO6310 touch screen?

Issue
Conformal coating option for HMIGTO6310

Product Line
Magelis

Resolution
Yes there is. The ordering part number for this Magelis touch screen that comes with conformal coating is HMIGTO6310FC.
Was this helpful?
What can we do to improve the information ?