Browse FAQs

Osisense XC - Data sheet of the XCLJ10514 limit switch

Published date: 19 October 2018

The XCLJ10514 limit switch does not have any data sheet on the "tesensors.com" site. It is in fact a red XCKJ10514 red painting, not visible in the commercial data base = ZCKJ1 red body Pg13 cable entry + ZCKE05 red head + ZCKY14 steel ball bearing mounted roller lever. Attached corresponding data sheet. Please note that the XCLJ10514 red switch is available to order in 2016. It is a MTO product (manufacture to order).


Was this helpful?

What can we do to improve the information ?

Can't find what you are looking for?

Reach out to our customer care team to receive information on technical support, assistance for complaints and more.