Technical FAQs

Ask a Question

Event Notification Module 8.3 Service Pack 2

Title
Event Notification Module 8.3 Service Pack 2

Issue
Event Notification Module 8.3 cannot retrieve alarms information

Product Line
Power Monitoring Expert (PME) 8.1
ENM 8.3

Environment
Any Power Monitoring Expert 8.1 system with Event Notification Module 8.3 or 8.3.1

Cause 
The timeout threshold in the designed dll file is being reached on some systems causing alarms to not be retrieved. 

Resolution
Hotfix and instructions are attached.
Was this helpful?
What can we do to improve the information ?