Technical FAQs

Ask a Question

Using a Third Party OPC Client to access PowerSCADA Expert Alarm Server Data

Issue
How to use a third party OPC client application, such as Matrikon, to access alarms.

Product Line
PowerSCADA Expert 8.1, PSE 8.1

Environment
OPC, OPCAE (Alarms and Events)

Cause
How to access the system and view alarm server data.

Resolution
To allow the third party application access: 

1. Select the project and run the Computer Setup Wizard.

2. On the General Options setup dialog select 'Register' . The Alarm server for that project is then registered and available for access via the third party application.

          

3. Run the third party application. From the list of available servers select Serck.ScxV6OPCAE..

4. Connect to the Server and depending on your third party application Create Event Subscription

All events will be listed.
Was this helpful?
What can we do to improve the information ?