Technical FAQs

Ask a Question

Can the Project Name displayed on the 'Home' webpage be changed ?

Title
Project Name displayed on the 'Home' webpage
 
Issue
Project Name displayed on the 'Home' webpage change
 
Product Line
M580
 
Environment
Unity Pro 11 or higher
 
Cause
N/A
 
Resolution
 Yes, the Unity project name that is displayed on the  Home webpage can be modified. To change a Unity 11 project name, open up the Project Properties and enter a new project name, rebuilt project and transferred program.After program transfer, the new project name is displayed after the webpage was refreshed.
Was this helpful?
What can we do to improve the information ?