Technical FAQs

Ask a Question

Preventa XY2C - How to set up the quick tensioner XY2CZ213 on the XY2CE or XY2CED rope pull switch

Please find attached the instructions to set up the quick tensioner XY2CZ213 on the XY2CE or XY2CED rope pull switch.
The tensioner(s) replace(s) the ring(s) supplied with the switch model.
Was this helpful?
What can we do to improve the information ?