Browse FAQs

Which meters comply with California Title 24 Meter Compliance?

Published date: 10 May 2019

Issue
Which meters comply with California Title 24 Meter Compliance? 

Product Line
Powerlogic and ION meters

Environment
Title 24 Compliance

Resolution

The California Title 24 Meter Compliance standards are as follows: 
 
Meter Type Services rated 50 kVA or less Services rated more than 50 kVA and less than 250 kVA Services rated more than 250 kVA and less than 1000 kVA Services rated more than 1000 kVA
Instantaneous kW demand Required Required Required Required
Historical peak demand (kW) Not required Not required Required Required
Resettable kWh Required Required Required Required
kWh per rate period Not required Not required Not required Required

Most Powerlogic/ION meters are suitable for Title 24. The acceptance of meters and the application design are contingent on the approval of the Authority Having Jurisdiction, according to their interpretation of the standard. 
 

Was this helpful?

What can we do to improve the information ?

Can't find what you are looking for?

Reach out to our customer care team to receive information on technical support, assistance for complaints and more.