Technical FAQs

Ask a Question

Which device types are supported with ComX driver in eSight software?

Issue
Which device types are supported with ComX driver in eSight software? 

Product Line
eSight version 2016.2, ComX driver 

Cause
List of device type supported with ComX driver in eSight software

Resolution
The ComX driver should support the following SE device types:

BCPM A (main and channel active energies - see graphic for how to import each channel current)


BCPM B (main active energy only)
EM3550
EM3555
iEM3455
iEM3555
PM5110
PM5330
PM5560
PM5563
Was this helpful?
What can we do to improve the information ?