Technical FAQs

Ask a Question

Osisense XC - Obsolete XCKB1D02 limit switch cross-reference

The obsolete XCKB1D02 limit switch can be replaced by the XCKJ167 or XCKJ167H29 limit switch. The tripping point A of the contact 21-22 changes from 2mm to 3.2mm by the 30° cam actuation. Differential travel changes from 0.5mm to 1.5mm.

                               
Was this helpful?
What can we do to improve the information ?