Technical FAQs

Ask a Question

Osisense XC - Obsolete XCKB1D01 limit switch cross-reference

The obsolete XCKB1D01 limit switch, having a end steel ball bearing plunger, can be replaced by the assembly ZCKJ1+ZCKE66 or ZCKJ1H29+ZCKE66 limit switch. The tripping point A of the contact 21-22 changes from 2mm to 3.2mm by the 30° cam actuation. Differential travel changes from 0.5mm to 1.5mm with the same actuation.

                           
Was this helpful?
What can we do to improve the information ?