Technical FAQs

Ask a Question

Osisense XC - Obsolete XCKB1D31 limit switch cross-reference

The obsolete XCKB1D31 limit switch can be replaced by the XCKJ10511 or XCKJ10511H29 limit switch. Tripping angle of the contact 21-22 changes from 18° to 23° by the 30° cam actuation.

                                  
Was this helpful?
What can we do to improve the information ?