Technical FAQs

Ask a Question

Does Schneider Electric offer a direct replacement for ILE1F661S2005 with ID number 66307190026 ?

No, the Lexium Intergated drive model ILE1F661S2005 with ID number 66307190026 is an OEM specific model which is not available directly from Schneider Electric.
Customers looking for ILE1F661S2005 with ID number 66307190026 must contact the OEM machine builder to attain the exact replacement type.

This model has a unique gearbox which is not offered in our catalog offer.
Only the OEM machine builder can provide the exact replacement motor assembly

 
Was this helpful?
What can we do to improve the information ?