Technical FAQs

Ask a Question

Unable to Modify Saved Report in PME

Issue:
A user modifies an existing saved report in the Web Applications, but after generating and saving the the changes, a second copy of the report is created. The original report is unmodified. 

Environment:
Web Applications
Reports

Product Line:
Power Monitoring Expert 8.x

Cause: 
This issue is caused when a user tries to modify a report created by another user account. Even when logged in with a Supervisor account, you can not modify another users report. Attempting to modify a report that another user created will result in a copy of that report being created instead (with the owner being the current user). 

Resolution:
To modify a report that was created by another user, you will need to have that user account make the modifications to the report. 
Was this helpful?
What can we do to improve the information ?