Technical FAQs

Ask a Question

Osisense XZ - XSZCA1501Y, XSZCA1502Y, XSZCA1503Y pre-wired 7/8"-16UN 5-pin straight connector replacement

The XSZCA1501Y (1.8m), XSZCA1502Y (4.6m), XSZCA1503Y (9.1m) pre-wired 7/8"-16UN 5-pin straight connectors, can be respectively replaced by the XZCPY1764L2 (2m), XZCPY1764L5 (5m), XZCPY1764L10 (10m) equivalent cabling accessory, PVC cable STOOW, yellow colour.
Attached :
- XSZCA150*Y details,
- XZCPY1764L2 data sheet.

XSZCA1502Y.jpg

                                                                            
Was this helpful?
What can we do to improve the information ?