Technical FAQs

Ask a Question

What is the operating temperature range of a Connexium Managed Dual Ring switch ?

Title
Connexium Managed Dual Ring switch operating temperature range
 
Issue
Connexium Managed Dual Ring switch operating temperature range
 
Product Line
Connexium
 
Environment
Ethernet
 
Cause
N/A
 
Resolution
The Operating temperature of the Connexium Managed Dual Ring switch (TCSESM_E) is  0 °C to +60 °C.
 
Was this helpful?
What can we do to improve the information ?