Technical FAQs

Ask a Question

M340 Program Download Error due to compatibility function list check failed issue

Title
M340 Program Download Error
 
Issue
M340 Program Download Error
 
Product Line
M340
 
Environment
Unity pro 11 or higher
 
Cause
N/A

Resolution
 The M340 connection error that states the following message, impossible to transfer due to compatibility (function list check failed) Any_Bool, indicates that the M340 needs a minimum version of the firmware.
The minimum firmware version required for the M340 CPU is OS version equal or > V2.70.
Your M340 CPU is probably using FW <2.70 and needs to upgrade it to the latest one (V 2.8) version.

 
Was this helpful?
What can we do to improve the information ?