Technical FAQs

Ask a Question

Osisense XC special - Cross-reference of the obsolete XF9JC1 overtravel power switch

The obsolete XF9JC1 (Ith = 260A) overtravel power switch, with manual resetting, is replaced by the XF9F1851 switch (Ith = 275A). Attached corresponding data sheet. The metal box of the new power switch has bigger dimensions than the obsolete enclosure. The arms of the new switch are longer than the old ones.

Was this helpful?
What can we do to improve the information ?