Technical FAQs

Ask a Question

Osisense XC special - Cross-reference of the obsolete XF9JC2 overtravel power switch

The obsolete XF9JC2 (Ith = 260A) overtravel power switch, with automatic resetting, is replaced by the XF9F1852 switch (Ith = 275A). Attached corresponding data sheet. The metal box of the new power switch has bigger dimensions than the obsolete enclosure. Arms have the same lenght.

Was this helpful?
What can we do to improve the information ?